AXIS#.MOTOR.BRAKEPOWERDELAY

Description

Time to wait after applying full voltage before dropping to low voltage when AXISx.MOTOR.BRAKEPOWERSAVING = 1.


  • This parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when MOTOR.AUTOSET=1 and motor memory version is 0.4 or greater.

Context

For more information see Brake and Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Milliseconds

Range

0 to 2000

Default Value

150

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen